yocto full build issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto full build issue

Jump to solution
14,926 Views
K_Varun
Contributor III

Hello Community

I'm trying to build the Yocto full build image of L6.1.22_2.0.0 in Ubuntu 20.04. using the build command : bitbake imx-image-full by following L6.1.22_2.0.0_LINUX_DOCS.

I am getting the bellow build error.

ERROR: Task (/home/user/imx/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc-locale_2.37.bb:do_package) failed with exit code '1'

attaching the complete build logs for your reference.

Please help me in solving this issue.

Thank you
 

0 Kudos
Reply
1 Solution
12,158 Views
K_Varun
Contributor III

Hello community,

adddng the below line in the local.conf has solved the issue for me.

GLIBC_GENERATE_LOCALES = "en_US.UTF-8" 

thanks
K Varun

View solution in original post

0 Kudos
Reply
10 Replies
14,883 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello @K_Varun 

Have you followed up the Yocto User Guide to set up "Essential Yocto Project host packages" on your build host?

Such as: 

sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential
chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils
iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev python3-
subunit mesa-common-dev zstd liblz4-tool file locales

 and sudo locale-gen en_US.UTF-8

 

Regards

Harvey

0 Kudos
Reply
14,880 Views
K_Varun
Contributor III

Hello @Harvey021 

Thank you for your response.

I have followed the Yocto Project documentation and installed all the essential host packages as recommended. For cross-verification, I also ran the sudo commands you provided earlier. However, the error still persists.

Could you please help me further investigate the issue?

Thank you for your assistance.

Best regards,

K Varun

 

0 Kudos
Reply
14,848 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @K_Varun 

I've tested the build on my host again, it works.

The build host: 22.04.1-Ubuntu

-b imx-linux-mickledore -m imx-6.1.22-2.0.0.xml

build_imx-image-full.png

Would suggest you to have a clean build and also check your system source, like the number of cores with the RAMs. 

 

Regards

Harvey

0 Kudos
Reply
14,856 Views
K_Varun
Contributor III

 

Dear Linux Community,

I am encountering an issue while building the image and need some assistance. Despite trying various approaches, I am still facing the following error during the build process: attaching the complete log-cat for better reference.

error: 

ERROR: glibc-locale-2.39+git-r0 do_package: oe_runmake failed
ERROR: glibc-locale-2.39+git-r0 do_package: ExecutionError('/home/user/imx/imx-yocto/build-xwayland/tmp/work/armv8a-poky-linux/glibc-locale/2.39+git/temp/run.oe_runmake.787591', 1, None, None)
ERROR: Logfile of failure stored in: /home/user/imx/imx-yocto/build-xwayland/tmp/work/armv8a-poky-linux/glibc-locale/2.39+git/temp/log.do_package.787591

 

I am following the steps provided in the READ ME for building the image, which can be found here: https://github.com/nxp-imx/imx-manifest.

Could anyone guide me on how to resolve this issue?

Looking forward to your help.

Best regards,

K Varun

0 Kudos
Reply
14,793 Views
K_Varun
Contributor III

Hello @Harvey021 

I’m still facing the glibc-locale error during the Yocto build process.

Here’s what I’ve tried so far:

  • Tested the build on both Ubuntu 22.04 and 20.04.
  • Verified all required build-essential packages.
  • Performed clean builds and reconfigured locale settings.
  • Followed your suggestions to clean the build and check system specs (32 GB RAM, 8 cores).

Unfortunately, the issue persists, and the build is still slow. Could you please suggest additional steps to resolve this? Also, do you have any recommendations on how to improve the build speed?

Thank you!

Best regards,
K Varun

0 Kudos
Reply
14,769 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @K_Varun 

Have a try to build glibc-locale separately before building any recipes or target.

the build speed mostly depends on the system sources and network bandwidth.

 

Regards

Harvey

0 Kudos
Reply
14,740 Views
K_Varun
Contributor III

Hello @Harvey021 

Tried to build only the glibc-locale separately before initiating the full build. however, the error still persists.

Attaching log- file for reference.

Regards 
K Varun

0 Kudos
Reply
12,522 Views
K_Varun
Contributor III

Hello Community,

Need your support to solve this gilbc-locale error. Facing this issue from long time.

Regards

K Varun

 

0 Kudos
Reply
12,287 Views
Harvey021
NXP TechSupport
NXP TechSupport

I believe that the problem mainly exists in your host. as said, we did test again in our host, no such issue.

 

Regards

Harvey

0 Kudos
Reply
12,159 Views
K_Varun
Contributor III

Hello community,

adddng the below line in the local.conf has solved the issue for me.

GLIBC_GENERATE_LOCALES = "en_US.UTF-8" 

thanks
K Varun

0 Kudos
Reply