yocto build full image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

yocto build full image

108 次查看
noway
Contributor I

hi,  community

# iMX 8MP

@ Harvey021

I missed a issue during builiding image,

build mechine docker: ubuntu 20.04

target image version: linux6.6.36 full

command: bitbake imx-image-full

I'm already copy the .git/* of matter to the path that calld "xxx/download/git2/github.com.NXP.matter.git/", but is it still showing fail fetch?

noway_0-1758176973151.png

 

0 项奖励
回复
1 回复

64 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

To the Expansion error, have you modified recipes or layers or other conf?

Please follow up the Yocto User Guide to rebuild the target.

To the error - unable to access, make sure that no network limit. Can try to manually bitbake -c fetch matter and build.

Here I just test bitbake imx-image-full for the same version of BSP without error.

 

Regards

Harvey

 

0 项奖励
回复