yocto build full image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto build full image

105 Views
noway
Contributor I

hi,  community

# iMX 8MP

@ Harvey021

I missed a issue during builiding image,

build mechine docker: ubuntu 20.04

target image version: linux6.6.36 full

command: bitbake imx-image-full

I'm already copy the .git/* of matter to the path that calld "xxx/download/git2/github.com.NXP.matter.git/", but is it still showing fail fetch?

noway_0-1758176973151.png

 

0 Kudos
Reply
1 Reply

61 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

To the Expansion error, have you modified recipes or layers or other conf?

Please follow up the Yocto User Guide to rebuild the target.

To the error - unable to access, make sure that no network limit. Can try to manually bitbake -c fetch matter and build.

Here I just test bitbake imx-image-full for the same version of BSP without error.

 

Regards

Harvey

 

0 Kudos
Reply