x11 rotation with reduced performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

x11 rotation with reduced performance

1,417 次查看
anjojohn
Contributor IV

Hi All,

Our device need to have landscape and portrait display settings. So far we set the x11 rotation with xorg and is working fine. x11 uses the vivante driver. But after rotation the performance is reduced and we can see increased cpu usage. We have touch interface which is also rotated with x11. Same issue was reported https://community.nxp.com/thread/351854 . Couldn't find any correct answer in which commit/release it was resolved. we are using the same 3.14 kernel and issue is there. 

This is very critical for us and would welcome any suggestions/answers

0 项奖励
回复
1 回复

1,168 次查看
b36401
NXP Employee
NXP Employee

As far as I know such rotation performance issue is fixed since 3.14.52 version.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复