MCIMX6ULL-EVK power consumption issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6ULL-EVK power consumption issue

546 Views
felixhsu
Contributor III

Hi All

The customer use MCIMX6ULL-EVK measurement power consumption on the deep sleep mode,

as below is CPU board result:

1. VDD_SOC_IN : 0.3mA
2. VDD_HIGH_IN : 0.1mA
3. DDR3L I/O : 7.0mA

with carrier board measurement result is "85mA", which device is consume big power on deep sleep mode? 

Thanks.

Labels (3)
0 Kudos
Reply
2 Replies

403 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  have You used recommendations of app note AN5345 (i.MX 6ULL Power

Consumption Application Note) ?

In particular - in sections

3.7. Measuring points on the MX6ULL EVK platform

6. Use case configuration and usage guidelines
6.1. Deep-Sleep mode

 

Results may be found in sections

4.1. Low-power mode use cases
4.1.1. Use case 1: Deep-Sleep mode (DSM)

https://www.nxp.com/docs/en/application-note/AN5345.pdf 

Have a great day,

Yuri

 ------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply

403 Views
felixhsu
Contributor III

Hi Yuri

 

The customer have follow AN5345.pdf, measurement result with 4.1.1. Use case 1: Deep-Sleep mode (DSM) Table 1 is close, but the result is SOC board without carrier board, the customer want to know why soc board with carrier board power consumption is so high, which device is power consume reason?

 

Thanks.

0 Kudos
Reply