Hi All,
I am trying to port cyw43455 wifi/bt on imx8mevk. I am able to figure out dts node for bluetooth porting pins but confused when porting wifi related configurations.
Below are the pin and port details I am using
wifi --> sdio
BT --> UART3.
| HMI NET NAME | IMX8 Pin name | 
| BT_REG_ON | NAND_CLE | 
| WL_REG_ON | NAND_CE2_B | 
| BT_HOST_WAKE | NAND_DQS | 
| BT_DEV_WAKE | NAND_CE1_B | 
| REF_CLK_32K | GPIO1_IO00 | 
| SD1_CMD | SD1_CMD | 
| SD1_DATA0 | SD1_DATA0 | 
| SD1_DATA1 | SD1_DATA1 | 
| SD1_DATA2 | SD1_DATA2 | 
| SD1_DATA3 | SD1_DATA3 | 
| SD1_CLK | SD1_CLK | 
| UART3_RXD | UART3_RXD | 
| UART3_TXD | UART3_TXD | 
| UART3_CTS | UART3_RXD | 
| UART3_RTS | UART3_TXD | 
| SAI5_RXD1 | L4 | 
| SAI3_TXFS | G3 | 
| SAI3_TXC | C4 | 
| SAI3_TXD | C3 | 
| SAI3_RXD | F3 | 
Here we are using both 1.8v for VIO and 3.3v for VBAT_LDO, but I don't have any clue how to configure VIO and VBAT in dts file. Please find attached dts prepared for above configuration. Please correct me if anything is wrong and help me how to add vio and vbat configuration in dts.
I find the same question at the Cypress forum (https://community.cypress.com/message/171931) has been answered correctly already.
Hello,
Have a look at Embedded Artists’ dts file on their github (https://github.com/embeddedartists/linux-imx/blob/ea_4.14.78/arch/arm64/boot/dts/freescale/fsl-imx8m...). Murata 1MW SDIO mode works fine with their IMX8MQ board.
You might also take a look at this post: https://community.nxp.com/thread/491236.
Hi Sandeep,
Am in same boat as you trying to bring up my sdio device , were you able to get the dts correct for the wifi? ok if you can share for a comparison.
Regards,
Sistla.
Am able to resolve this issue after finding and resolving issues on the SDIO device side