I want to work SDMA with EIM on iMX6, but i didn't found that
anyone knows?
I'm using linux kernel 3.0.15
已解决! 转到解答。
OK, we only have one way : using SW to start SDMA.
Let me see how to !
Customers can send me email to ask for example code on how to use SDMA on WEIM interface !
At same time , Please provide project information.
Email : weidong.sun@freescale.com
在原帖中查看解决方案
Hello Weidong, send me the example code SDMA and EIM dma mem transfer.
My email: fhx9999@163.com
Thanks!!!
Hi weidong:
We need to transfer data over eim from fpga to imx6q processor.
Can you send me the example code for SDMA?
My email: dubovkin.as@gmail.com
Dear Weidong:
I also want to test the mem to mem transfer using SDMA, Could you please send me the example code.
My email: jasper.nuytten@basalte.be
thanks a lot!
Weidong Sun
你好 我是一个中国学生,你我现在在做一个项目会用到EMI接口和FPGA通信,打算采用DMA通信的方式,但是现在遇到一个问题,在测试的时候总线上没有任何信号发生,希望你能发给我一个例程,非常感谢。我的邮箱是bujigr@163.com
郭瑞
Hello Weidong,
I want use SDMA replace memcpy.
please send the examples to me too.
I'm using linux kernel 3.0.35.
my email:liangweilin@nearbylink.com
Thanks!
Hi Weidong Sun,
I would like to know if you can send me an exemple of SDMA and EIM at aurelien.grange@rsautomation.com
Does someone know hox to set EIM clock at 104MHz (to perform SDMA)?
Thanks
Hi Weidong:
could you please send me a copy of MEM TO MEM sdma codes to sales.edgepbx@gmail.com
Thank you very much
Could you please send me a copy of MEM TO MEM SDMA code to rziemins@lgsinnovations.com
I would also like to have te sample code.
My email is victor.osornio@freescale.com
My email: garam308@gmail.com
My email: lijian@tigergroup.cn
Hello,All,
Those friends who recieved Email on WEIM mem to mem help me to press correct answer button !
weidong
Could you also send the sample code to me ? My email: cloundliu@163.com
Hi Weidong,
Can you please send me the example code for SDMA for MEM to MEM transfer?
I'm using the linux version : linux-3.0.35
My mail id :togw2001@yahoo.co.jp
Regards,
Toshiaki Ogawa
My email: hyunjaiyaa@naver.com
Could you also send the sample code to me ?
My email is: snlee@tgate.co.kr
Regards
Seok-nam
I would appreicate if if you could forward the sample code to me.
regards
Pat
Could you also send the sample code to me too?
My email is: stevolution84@gmail.com
Dear Weidong,
Could you also send the sample code to me?
Mail:song_lin@microjet.com.tw
Song_Lin