wifi driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wifi driver

9,537 Views
Danial
Contributor II
The default wifi driver of the system is ar6000, but I want to use the 8686 device. How to configure the system? I have configured the kernel and the kernel can load 8686 drive corretly. I also modified the Boardconfig.mk , init.rc ,wifi.c In device/fsl/imx53_logo/Boardconfig.mk: #WIFI_DRIVER_MODULE_NAME := "ar6000" #WPA_SUPPLICANT_VERSION := VER_0_6_ATHEROS WPA_SUPPLICANT_VERSION := VER_0_6_X #BOARD_WLAN_ATHEROS_SDK := system/wlan/atheros/AR6kSDK #BOARD_WPA_SUPPLICANT_DRIVER := AR6000 BOARD_WLAN_CHIP_AR6102 := true BOARD_WLAN_CHIP_AR6003 := true BOARD_WPA_SUPPLICANT_DRIVER := WEXT # Select Wake on wireless mode for AR6003 suspend/resume policy BOARD_WLAN_PM_SUSPEND := 2 In the device/fsl/imx53_logo/Init.rc, I commented out the sentences. #service wpa_supplicant /system/bin/wlan_tool wpa_supplicant # socket wpa_wlan0 dgram 660 root wifi # disabled # oneshot #service wlan_tool /system/bin/wlan_tool # oneshot In the device/fsl/imx5x/init.rc, I modified some places. # give system access to wpa_supplicant.conf for backup and restore mkdir /system/etc/wifi 0770 wifi wifi chmod 0770 /system/etc/wifi chmod 0660 /system/etc/wifi/wpa_supplicant.conf chown wifi wifi /system/etc/wifi/wpa_supplicant.conf #wpa_supplicant control socket for android wifi.c (android private socket) mkdir /data/misc/wifi 0770 wifi wifi mkdir /data/misc/wifi/sockets 0770 wifi wifi chmod 0770 /data/misc/wifi chmod 0660 /data/misc/wifi/wpa_supplicant.conf chown wifi wifi /data/misc/wifi chown wifi wifi /data/misc/wifi/wpa_supplicant.conf service wpa_supplicant /system/bin/wpa_supplicant -dd -Dwext -iwlan0 -c /system/etc/wifi/wpa_supplicant.conf socket wpa_wlan0 dgram 660 wifi wifi group system wifi inet disabled oneshot In the hardware\libhardware_legacy\wifi\wifi.c, I modified some places. #else /* ATHENV */ #ifndef WIFI_DRIVER_MODULE_PATH #define WIFI_DRIVER_MODULE_PATH "/system/lib/modules/libertas_sdio.ko" #endif #ifndef WIFI_DRIVER_MODULE_NAME #define WIFI_DRIVER_MODULE_NAME "libertas_sdio" #endif #ifndef WIFI_DRIVER_MODULE_ARG #define WIFI_DRIVER_MODULE_ARG "" #endif #ifndef WIFI_FIRMWARE_LOADER #define WIFI_FIRMWARE_LOADER "" #endif #define WIFI_TEST_INTERFACE "wlan0" #endif In the external\wpa_supplicant_6\wpa_supplicant\wpa_supplicant.conf, I modified some place. ctrl_interface=wlan0 I think the system use the Android private socket, but I am not sure. After I run the system, the error come out. I have attached the log file. Thanks!
Labels (1)
0 Kudos
Reply
5 Replies

5,942 Views
Swamy
Fresh Out Contributor

Hi Zhoudan,

I am facing similar issue. Can you share if you have found any solution.

Regards,

Swamy

0 Kudos
Reply

5,942 Views
admin
Specialist II

Actually your unable to find the interface wlan0 (I am also facing the same problem).If anyone found the solution.

please help us out.

Thanks,

prannoy.

0 Kudos
Reply

5,942 Views
Danial
Contributor II

移植wifi驱动MX53平台

配置内核支持8686wifi

选上Networking support->wireless->cfg80211 – wireless configuration API

选上Device Drivers->Network device support->Wireless LAN->Marvell 8xxx Libertas WLAN driver support->Marvell Libertas 8385/8686/8688 SDIO 802.11b/g cards

修改hardware\libhardware_legacy\wifi\wifi.c

//#define WIFI_TEST_INTERFACE             "sta"

#define WIFI_TEST_INTERFACE                "wlan0"

在rmmod函数中直接返回,如下代码:

static int rmmod(const char *modname)

{

    int ret = -1;

    int maxtry = 10;

return 0;

…...

}

配置wpa_supplicant的驱动Z:\myandroid\device\fsl\imx53_smd\BoardConfig.mk

#---------------------------------------------------------------

#WIFI_DRIVER_MODULE_NAME     := "ar6000"

#WPA_SUPPLICANT_VERSION      := VER_0_6_ATHEROS

#BOARD_WLAN_ATHEROS_SDK      := system/wlan/atheros/AR6kSDK

#WPA_SUPPLICANT_VERSION      := VER_0_6_ATHEROS

#BOARD_WPA_SUPPLICANT_DRIVER := AR6000

BOARD_WLAN_CHIP_AR6102 := false

BOARD_WLAN_CHIP_AR6003 := false

#BOARD_WPA_SUPPLICANT_DRIVER := WEXT

# Select Wake on wireless mode for AR6003 suspend/resume policy

#BOARD_WLAN_PM_SUSPEND       := 2

WIFI_DRIVER_MODULE_NAME     := "libertas_sdio"

WIFI_DRIVER_MODULE_PATH     := "/system/lib/modules/libertas_sdio.ko"

BOARD_WIFI_LIBRARIES := true

BOARD_WPA_SUPPLICANT_DRIVER := WEXT

WPA_BUILD_SUPPLICANT := true

WPA_SUPPLICANT_VERSION := VER_0_5_X

#-----------------------------------------------------------------

修改wpa_supplicant.conf

把external/wpa_supplicant/wpa_supplicant.conf拷贝到/system/etc/wifi/目录下,
并把:ctrl_interface=DIR=/data/misc/wifi/wpa_supplicant GROUP=wifi
改为:   ctrl_interface= /data/system/wpa_supplicant //这个一定要和IFACE_DIR对应并保证目录权限

配置路径和权限:\myandroid\device\fsl\imx5x\init.rc

# give system access to wpa_supplicant.conf for backup and restore

#--------------------------------------------

    mkdir /system/etc/wifi 0777 wifi wifi

         chmod 0777 /system/etc/wifi

         chmod 0777 /system/etc/wifi/wpa_supplicant.conf

         chown wifi wifi /system/etc/wifi/wpa_supplicant.conf

                  

         mkdir /data/misc/wifi 0777 wifi wifi

         mkdir /data/misc/wifi/sockets 0777 wifi wifi

         chmod 0777 /data/misc/wifi

         chown wifi wifi /data/misc/wifi/wpa_supplicant.conf

         chown wifi wifi /data/misc/wifi

         chmod 0666 /data/misc/wifi/wpa_supplicant.conf

   

    mkdir /data/system/wpa_supplicant

    chmod 0777 /data/system/wpa_supplicant

    chown wifi system /data/system/wpa_supplicant

#--------------------------------------------

# Prepare for wifi

    mkdir /data/misc/dhcp 0770 dhcp dhcp

    chown dhcp dhcp /data/misc/dhcp

    setprop wifi.interface wlan0

    setprop wlan.interface wlan0

修改\myandroid\device\fsl\imx53_smd\init.rc

注释掉原有的:

#service wpa_supplicant /system/bin/wlan_tool wpa_supplicant

#    socket wpa_wlan0 dgram 660 root wifi

#    disabled

#    oneshot

#service wlan_tool /system/bin/wlan_tool

#    oneshot

加入以下语句:
#------------------------------------------------------------------------------------------------------------------------

service wpa_supplicant /system/bin/wpa_supplicant -Dwext -iwlan0 -c /data/misc/wifi/wpa_supplicant.conf

    socket wpa_wlan0 dgram 0666 wifi wifi

    disabled

    oneshot

service dhcpcd /system/bin/logwrapper /system/bin/dhcpcd -o domain_name_servers -ABKL

         disabled

         oneshot

         group system dhcp

on property:init.svc.wpa_supplicant=stopped

         stop dhcpcd

#------------------------------------------------------------------------------------------------------------------------

提供固件firmware

Android不使用标准的hotplug binary,WIFI需要的firmware要复制到/etc/firmware。   或者复制到WIFI驱动指定的位置,然后WIFI驱动会自动加载.

在此把wifi模块提供的sd8686.bin sd8686_helper.bin放到/system/etc/firmware目录下。


This is the solution,I get my wifi worked successfully.


0 Kudos
Reply

5,942 Views
phuongdangminh
Contributor III

Hello danzhou,

I've follow your guide but it didn't work. May I have some questions

1> What kernel linux which you're using ?

2> What is libertas firmware version ?

When turning on the WIFI, the wpa_supplicant said not support wext driver, have we to modify this driver ?

Many thanks for your help.

0 Kudos
Reply

5,942 Views
phuongdangminh
Contributor III
0 Kudos
Reply