i.MX287 PMU without battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX287 PMU without battery

Jump to solution
1,346 Views
matthewforce
Contributor I

I am using an i.MX287 in an application where it is powered from 5V and does not use a battery.  How should the PMU pins associated with the battery (BATTERY, DCDC_BATT, etc) be tied?

Thanks,

Matt

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
901 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Matt,

Please see page 4 of the attached, it shows all the connections for 5V only operation. MX23 PMU is the same as MX28.

Best regards.

Jorge.

View solution in original post

0 Kudos
Reply
1 Reply
902 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Matt,

Please see page 4 of the attached, it shows all the connections for 5V only operation. MX23 PMU is the same as MX28.

Best regards.

Jorge.

0 Kudos
Reply