Hi i.MX Community,
Use source code of fsl-release-bsp-imx-3.10.17-1.0.0_ga,failed play video through command "gplay akiyo.mp4" (example: /unittest/akiyo.mp4).Can you tell me how to resovle it?
BTW,If use mplayer tool,that playing ok.
Refer to imx6q_sabresd board.
Thanks!
Best Regards
Eason
已解决! 转到解答。
Hi Eason
please try latest BSP
L3.14.28_1.0.0_iMX6QDLS_BUNDLE 
 : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo
Linux Binary Demo Files and Linux BSP Documentation
Size (K): 1479000 Format: gz Rev #: L3.14.28_1.0.0 Modified: 4/10/2015
3.10.17 is removed from i.MX6QD official product web page, so it is not more supported
i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Eason
please try latest BSP
L3.14.28_1.0.0_iMX6QDLS_BUNDLE 
 : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo
Linux Binary Demo Files and Linux BSP Documentation
Size (K): 1479000 Format: gz Rev #: L3.14.28_1.0.0 Modified: 4/10/2015
3.10.17 is removed from i.MX6QD official product web page, so it is not more supported
i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------