i.MX6DL SABRE-AI board, EIM and USB_OTG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL SABRE-AI board, EIM and USB_OTG

Jump to solution
740 Views
jeevanmahadevu
Contributor II

With reference to i.MX6DL SABRE-AI board,

1. How is EIM DA0 - DA15 and EIM A16 - A24, can be used both by boot configuration select and by 32MB NOR Flash ?

2. USB_OTG_VBUS / USB_ID how to handle these when USB OTG is used as serial downloader port during the boot.

Can USB_ID be unconnected for the above application with the connector being micro_USB_AB

Thank you

0 Kudos
Reply
1 Solution
679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

1. for usage of these signals one can  check Figure 2-1. Boot configuration

   for development mode IMX6DQ6SDLHDG

2. USB_ID is not checked by serial downloader, USB_OTG_VBUS

   should be provided from USB connector.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
680 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

1. for usage of these signals one can  check Figure 2-1. Boot configuration

   for development mode IMX6DQ6SDLHDG

2. USB_ID is not checked by serial downloader, USB_OTG_VBUS

   should be provided from USB connector.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply