why I.MX6 Dual/Quad does not support renderscript?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why I.MX6 Dual/Quad does not support renderscript?

Jump to solution
2,650 Views
granttao
Contributor III

I.mx6 dual/quad has a gc2000 gpu from vivante, vivante's engineer said GC2000/GC4000 support renderscript (http://www.socip.org/socip/speech/pdf/2-Vivante-SoCIP%202011%20Presentation.pdf),   

anybody know why why I.MX6 Dual/Quad does not support renderscript?  ( the datasheet says nothing about renderscript).

as many I.MX6 Dual/Quad chips will be operated by android, that is not good choice, i think.

Labels (4)
Tags (2)
0 Kudos
Reply
1 Solution
2,212 Views
PrabhuSundarara
NXP Employee
NXP Employee

I.MX6 Dual/Quad supports renderscripts. i.MX6X has support for Android ICS and JB.  renderscript is natively supported in the Android.

View solution in original post

0 Kudos
Reply
2 Replies
2,213 Views
PrabhuSundarara
NXP Employee
NXP Employee

I.MX6 Dual/Quad supports renderscripts. i.MX6X has support for Android ICS and JB.  renderscript is natively supported in the Android.

0 Kudos
Reply
2,212 Views
granttao
Contributor III

Thank you very much, Prabhu.

Maybe i did not state my question clearly. Renderscript is only a runtime api from google, it can run on any platform (CPU, GPU, DSP), ICS and JB have little connection with renderscript, most of their graphic smoothness are archived by using OpenGL ES 2.0.

What i mean is why freescale did not worked with google to develop a renderscript runtime evironment which would use the GC2000 GPU for general purpose computing.

I have carefully checked the mx6 D/Q's  android demo image, the renderscript runtime lib (librs.so) is the general version provided by google. So, the mx6 d/q does have a driver for renderscript gpu computing. Maybe vivante can provide the driver?

thanks a lot

0 Kudos
Reply