where uboot source code is put in?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where uboot source code is put in?

2,042件の閲覧回数
mingmingyuan
Contributor III

linux 3.0.35  ltlib manger

I can't find uboot source code,can you tell me where uboot source code path?

thanks

ラベル(2)
0 件の賞賛
返信
1 返信

1,934件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mingming

please refer to p.10 attached Linux Guide:

Get the source code of one package.

The source code will be extracted to <ltib folder>/rpm/BUILD/ */

./ltib -m prep -p <package name>

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信