where peripheral port address imx6 imx7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

where peripheral port address imx6 imx7

1,281 次查看
fatalfeel
Contributor V

where is the peripheral port address(PERIPHERAL remap address) on imx6d imx6q and imx7 of android 6.0

for read peripheral port address to r0 use

mcr p15,0,r0,c15,c2,4

标签 (2)
0 项奖励
回复
2 回复数

1,206 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jesse

please check

"What is the Peripheral Port Remap Register for ?
Applies to: ARM1136, ARM1176"

ARM Information Center 

also may be useful to look at linux/arch/arm/mach-imx/hardware.h,mx6.h,mx7.h

linux-2.6-imx.git - Freescale i.MX Linux Tree 

linux-2.6-imx.git - Freescale i.MX Linux Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,206 次查看
fatalfeel
Contributor V

so imx6d q do not have this PERIPHERAL port address right?

0 项奖励
回复