where peripheral port address imx6 imx7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where peripheral port address imx6 imx7

1,268件の閲覧回数
fatalfeel
Contributor V

where is the peripheral port address(PERIPHERAL remap address) on imx6d imx6q and imx7 of android 6.0

for read peripheral port address to r0 use

mcr p15,0,r0,c15,c2,4

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,193件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jesse

please check

"What is the Peripheral Port Remap Register for ?
Applies to: ARM1136, ARM1176"

ARM Information Center 

also may be useful to look at linux/arch/arm/mach-imx/hardware.h,mx6.h,mx7.h

linux-2.6-imx.git - Freescale i.MX Linux Tree 

linux-2.6-imx.git - Freescale i.MX Linux Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,193件の閲覧回数
fatalfeel
Contributor V

so imx6d q do not have this PERIPHERAL port address right?

0 件の賞賛
返信