where is scatter-loading description

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

where is scatter-loading description

2,559 次查看
fatalfeel
Contributor V

where is the scatter-loading description in i.mx6

whats the file name

I need change it for long branch~~~

标签 (2)
0 项奖励
回复
6 回复数

2,318 次查看
fatalfeel
Contributor V

ok i find the topic
scatter file

where is freescale's scatter file location?
how to generate it?

0 项奖励
回复

2,318 次查看
Yuri
NXP Employee
NXP Employee

Hi,

The simpest scatter file mau be found at

c:\Program Files\DS-5 v5.21.0\examples\Bare-metal_boards_examples.zip\DS-5Examples\Freescale-iMX6Q_RAM\scatter.scat

It uses internal RAM of i.MX6. You may change it for external DRAM, just changing

base address from 0x0090_0000 to 1000_0000, assuming initialization script provides

DRAM controller (MMDC) settings.

 


Regards,

Yuri.

0 项奖励
回复

2,318 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Please let me know more details about the problem.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,318 次查看
fatalfeel
Contributor V

thanks Yuri

ARM Information Center
i want to do long call/jump arm said edit scatter-loading description
but where is it? must have a file name or location

0 项奖励
回复

2,318 次查看
fatalfeel
Contributor V

Scatter-loading description file

The scatter-loading description file syntax shown in the following figure reflects the functionality provided by scatter-loading itself:ARM Information Center

0 项奖励
回复

2,318 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The scatter file depends on memory, used by an application.

An example for internal memory (OCRAM) may be found in attachment

of the following thread.

Integrating Processor Expert for i.MX and ARM GCC with Eclipse

General memory map of i.MX6 is described in Chapter 2

(Memory Maps) of the i.MX6 D/Q Reference Manual.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Regards,

Yuri.

0 项奖励
回复