when the android5.1.1 will be release?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when the android5.1.1 will be release?

1,162 Views
wilsonchen
Contributor III

I use the i.mx6dq board,I want to know when the android5.1.1 should be released.

I found the L5.1.1_2.0.0_6qp-ga  on the FSL git server.  the release?

Labels (6)
0 Kudos
Reply
1 Reply

1,044 Views
igorpadykov
NXP Employee
NXP Employee

Hi wilson

it is planned on 1Q16

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply