what processor mounted on Sabre Board (MCIMXABASEV1)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what processor mounted on Sabre Board (MCIMXABASEV1)?

990件の閲覧回数
jaden
Contributor I

I have MCIMXABASEV1 board (SABRE for Automotive Infotainment Based on the i.MX 6 Series)

I want to know about specification of this board, but I cant find it T.T

I found specification below "

Processor

i.MX 6QuadPlus processor running up to 1 GHz, i.MX 6Quad processor running up to 1 GHz or i.MX 6Dual Lite processor running up to 800 MHz
* i.MX 6QuadPlus, i.MX 6Quad and i.MX 6Dual Lite can be configured as an i.MX 6DualPlus, i.MX 6Dual, and i.MX 6Solo processor for lower CPU load applications

 

but, I dont know what processor used for this board yet... (i.mx 6quad? i.mx 6dual lite?)

anyone knows? how find the processor mounted on my board?

ラベル(1)
0 件の賞賛
返信
1 返信

935件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The MCIMXABASEV1 is base board, is the i.MX 6Quad/6Dual/6DualLite/6Solo Expansion Board. You need the CPU card, you can see which CPU card on your side.SABRE|Automotive-Infotainment|i.MX6 | NXP 

0 件の賞賛
返信