what is the boot argument to load UBUNTU binary image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the boot argument to load UBUNTU binary image

1,017 Views
VadivelmuruganR
Contributor I

Dear All,

          I want to launch iMX50_Ubuntu_Demo_Image.bin on i.MX50 QSB ,I can able to copy by using DD

command .but freescale did not given any boot parameters ,If any one knows it would be appreciatable.

Thanks

Muruagn 

Tags (1)
0 Kudos
Reply
1 Reply

958 Views
PeterChan
NXP Employee
NXP Employee

The boot parameters are already set in the demo image. Just dd the the image to your SD card from the first sector and the card is ready to boot. By default, the display device is "hdmi".

To inspect and change the boot parameter, just hit any key in your serial console to stop the auto boot countdown and then type the command "printenv".

0 Kudos
Reply