what OS could be installed on i.MX5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what OS could be installed on i.MX5

1,184 次查看
borune
Contributor I

hello,

i've never worked with nxp products before and need a little help and explanation. Now i have a i.mx6 and need to create stream server based on it. For achieving that i want to use vlc. I have some questions.
1. What operation system i.mx6 has on board?
2. Could i get vlc binaries from anywhere for running vlc on this board?
3. If there are no repos can vlc be built from sources?
4. How can i build binaries? Are there gcc/g++ compilers or i should do cross-compiling?

Thanks

标签 (1)
2 回复数

1,053 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Boris Boris,

(1) There are currently BSPs for both Linux and Android for the i.MX6. You can find more information about each on the following links:

Embedded Linux for i.MX Applications Processors

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/em...

Android OS for i.MX Applications Processors

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/an...

(2) As for VLC I haven’t tested it but there is a vlc recipe on the OpenEmbedded layer for the Yocto Linux BSP. I would recommend downloading the documentation for the Linux BSP (preferably the latest release) and following it. Once you have the Yocto environment setup you can customize the images an add additional packages like vlc.

(3) Please note that the VLC recipe is part of the Yocto Project and it’s not maintained by NXP. You may find the recipe on the Open Embedded layer. There is some more information on the link below:

https://layers.openembedded.org/layerindex/branch/master/layer/meta-multimedia/

(4) If you wish to build binaries outside the Yocto or Android BSP you may use the GCC toolchain. The version of the toolchain would depend on the BSP being used. You may actually extract the toolchain from the Linux BSP using the following command within the Yocto environment:

$ bitbake meta-toolchain

This will create a script that will install the toolchain for the selected MACHINE.

I hope this helps!

Regards,

1,053 次查看
borune
Contributor I

thanks, gusarambula

0 项奖励
回复