warning while executing iwconfig on imx6sololite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

warning while executing iwconfig on imx6sololite

2,791 Views
mutyalaraoneela
Contributor III

Hi all,

I have cross compiled my driver and able to insert it perfectly but after that when I execute the command "iwconfig"

to know the status of my device I am ending up with the warning:

Warning: Driver for device wifi1 has been compiled with an ancient version

of Wireless Extension, while this program support version 11 and later.

Some things may be broken...

Platform details:

i.MX6 sololite with 3.10.17 kernel , yocto build.

Please guide me to move ahead.

Thanks and Regards,

Mutyala rao.

Labels (5)
0 Kudos
Reply
5 Replies

2,546 Views
susangracerapak
Contributor II

Hi ,

Please help me to fix this issue?

Regards

Susan

0 Kudos
Reply

2,546 Views
vikaskolapudi
Contributor I

Hi All,

Can anybody help me regarding this issue?

Thanks & Regards,

Joseph Vikas.

0 Kudos
Reply

2,546 Views
mutyalaraoneela
Contributor III

Hi Victor,

Thank you for the reply.

Please find the attachment for the Output of iwconfig command. iwconfig.png

I need the output to be displayed properly to see the ESSID, MAC, Frequency and Encryptioin keys etc..., so, I need this command to work.

Please suggest me how to proceed.

Thanks and Regards,

Mutyalarao.

0 Kudos
Reply

2,546 Views
mutyalaraoneela
Contributor III

Hi All,

Along with iwconfig, iwpriv is also not working fine.If I enable wireless extensions in the kernel, then I am facing some lockdep dependencies due to that unknown symbols are coming when I installed my wlan driver.

Any help is appreciated.

Thanks and Regards,

Mutyalarao.

0 Kudos
Reply

2,546 Views
b36401
NXP Employee
NXP Employee

It is just a warning that your driver uses old version of the protocol.

Usually it does not affect its main functions.

However you may try to find more recent sources to make the driver more precise.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply