Noisy green lateral band when using imxipuvideotransform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Noisy green lateral band when using imxipuvideotransform

532 Views
rodolfogiometti
Contributor I

Hello,

I'm using gstreamer-imx on my IMX6Q based board running Debian with the following command line:

gst-launch-1.0 -v filesrc location=pansy-1280x720-565.rgb blocksize=1843200 ! videoparse width=1280 height=720 framerate=5/1 format=29 ! decodebin ! imagefreeze ! imxipuvideotransform ! video/x-raw,format=I420 ! imxvpuenc_mpeg4 ! queue ! rtpmp4vpay ! udpsink host=192.168.32.42 port=5000

The command takes a static RGB565 image, then calls the imxipuvideotransform plugin and sends the result to my host PC over the network where I use the command below to see the image:

gst-launch-1.0 udpsrc port=5000 caps = "application/x-rtp, media=(string)video,clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)4,config=(string)000001b004000001b59113000001000000012000c888800cd28045a14103, payload=(int)96,ssrc=(uint)3938653480, timestamp-offset=(uint)2667048504, seqnum-offset=(uint)31662" ! rtpmp4vdepay ! avdec_mpeg4 ! autovideosink sync=false

Everything works well but a noisy green lateral band on the host PC output window! However, if I use the same command as above on my IMX6Q board but replacing the plugin imxipuvideotransform with the standard videoconvert then the band disappears and the output is perfect.

Any advice in order to fix this issue?

Thanks in advance,

Rodolfo

0 Kudos
2 Replies

319 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rodolfo

gstreamer-imx is developed and supported by community,

difference between community GStreamer-imx plugins and

Freescale GStreamer Plugins (fsl-gst-plugin package) can be found on

trac.gateworks.com/wiki/Yocto/gstreamer

so one can post it on meta-fsl-arm mailing list, so that someone familiar with

it could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Alternatively one can try fsl-gst-plugins, please check attached Release Notes

Table 6. Multimedia standard packages

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

319 Views
rodolfogiometti
Contributor I

Hi Igor,

thanks for your answer. However I ned to execute gstreamer on a Debiam. Is there any change about the possibility to execute the Freescale GStreamer Plugins on a Debian OS instead of Yocto?

Thanks in advance,

Rodolfo

0 Kudos