Hi,
Play video for long time, system crash and show vpu blocking timeout log.
Kernel: 3.0.35 android:4.2.2
Log:
----------------------------------------------------------------------------------------------------------
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = d0024000
[00000000] *pgd=00000000
Internal error: Oops: 80000005 [#1] PREEMPT SMP
Modules linked in:
CPU: 0 Not tainted (3.0.35 #194)
PC is at 0x0
LR is at __schedule+0x2ac/0x788
pc : [<00000000>] lr : [<c06499f0>] psr: 60000013
sp : d024bf30 ip : d024bec8 fp : 00000001
r10: ffffffff r9 : 00000001 r8 : 00000010
r7 : d01586c0 r6 : 40568d30 r5 : d024a000 r4 : 00000010
r3 : d41fe440 r2 : 00000000 r1 : d4202420 r0 : fffffffc
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c53c7d Table: 2002404a DAC: 00000015
LR: 0xc0649970:
9970 e5973160 e0223003 e1b03423 1a0000af e59f3534 e597216c e593316c e1520003
9990 1a0000a7 e5970024 e1a01007 e2800205 ebe8326d e59530f0 e1a00005 e3530000
99b0 058530f4 05849494 e51b9090 e5951004 e5992004 ebe7fbb2 e1a01000 e5963014
99d0 e307cf40 e34cc088 e51b8080 e3079f40 e34c9088 e79c0103 e0880000 ebe8aa59
99f0 e5963014 e7994103 e0884004 e59434bc e3530000 1a00001f e5962000 e5963004
9a10 e3120002 e2433001 e5863004 1affff55 e24bd020 e8bd8ff0 e1570009 1affffc8
9a30 eaffffdb e5953000 e3130081 0a000003 e5952004 e5922000 e3120001 1a000106
9a50 e3a02001 e1a00004 e1a01005 ebe8b0d8 e595300c e3a02000 e585201c e3130020
SP: 0xd024beb0:
beb0 d01586c0 00000000 00000001 00000000 00000000 c064b330 d01eac6c 00000000
bed0 d024bf08 0000040f 00000005 40568d30 d01586c0 c00484d4 fffffffc d4202420
bef0 00000000 d41fe440 00000010 d024a000 40568d30 d01586c0 00000010 00000001
bf10 ffffffff 00000001 d024bec8 d024bf30 c06499f0 00000000 60000013 ffffffff
bf30 00000000 00000000 00000001 00000001 d41985a0 00000000 00004bc5 00000000
bf50 c08ee930 c08740c0 a8727958 04b91373 00000000 00000010 40568d30 00000001
bf70 d41fe440 c007cc28 d4198588 d4198588 00000008 41443548 ffffffff 00000000
bf90 000000fc c0048a84 d024a000 00000000 00000000 c0048900 41443548 ffffffff
IP: 0xd024be48:
be48 c00401b4 c0041320 00000780 00000001 00000780 00000d80 00000000 00000438
be68 00000020 00000000 00000000 00000008 00000000 00000008 00000008 00000000
be88 00000010 00000008 00000000 00000018 00000008 00000000 00000000 00000000
bea8 d024a000 00000000 d01586c0 00000000 00000001 00000000 00000000 c064b330
bec8 d01eac6c 00000000 d024bf08 0000040f 00000005 40568d30 d01586c0 c00484d4
bee8 fffffffc d4202420 00000000 d41fe440 00000010 d024a000 40568d30 d01586c0
bf08 00000010 00000001 ffffffff 00000001 d024bec8 d024bf30 c06499f0 00000000
bf28 60000013 ffffffff 00000000 00000000 00000001 00000001 d41985a0 00000000
R1: 0xd42023a0:
23a0 00000000 00000000 00000000 00000001 00000000 00000000 d42023b8 d42023b8
23c0 00000000 d42023c4 d42023c4 00000000 00000000 c0083a10 00000000 00000000
23e0 00000000 00000000 00000000 00000000 0000c350 0000c350 00000000 00000000
2400 00000000 00000000 00000000 00000000 00080010 00000000 00000000 d42024b0
2420 00000001 d038a000 00000002 00400040 00000000 00000000 00000000 00000000
2440 0000006f 0000006f 0000006f 00000000 c064e220 00000000 00001dc4 000899bc
2460 00000001 00000000 00000000 d420246c d420246c 00000000 f4da5296 00000667
2480 d4439b53 0000000a d91f7341 00003051 d4429d6b 0000000a 0000376e 00000000
R3: 0xd41fe3c0:
e3c0 00000000 00000000 00000000 00000001 00000000 00000000 d41fe3d8 d41fe3d8
e3e0 00000000 d41fe3e4 d41fe3e4 00000000 00000000 00000000 00000000 00000000
e400 00000000 00000000 00000000 00000000 0000c350 0000c350 00000000 00000000
e420 00000000 00000001 00000001 00000000 d41fec88 d41fe3f8 d439c844 00000000
e440 00000000 d024a000 00000002 00400040 00000000 00000000 00000001 00000001
e460 00000070 00000070 00000070 00000000 c064e220 00000000 000017d4 000abe5d
e480 00000001 d44097a8 00000000 d4289250 d4289250 00000001 fcd4f741 00000667
e4a0 b9446193 00000033 da73f902 00003051 b1c15230 00000033 0000125a 00000000
R5: 0xd0249f80:
9f80 ffffff9c 00000001 00000000 00000000 00000000 00000000 0000008e c0048a84
9fa0 00000000 c0048900 00000000 00000000 0000000f 40580e24 00000000 00000000
9fc0 00000000 00000000 00000000 0000008e 400c1858 400c1858 00000001 0000000e
9fe0 40580de8 40580dd8 400c04e5 4015112c 00000010 0000000f ffffffff ffffffff
a000 00000000 00000002 00000000 d41fe440 c089e03c 00000000 00000015 c1269320
a020 d41fe440 d024a000 d5cf38a0 c00401b4 ce157820 00000000 d024bcfc d024bc58
a040 c06499c8 00000000 00000000 00000000 00000000 00000000 01010000 00000000
a060 40568f00 00000000 00000000 00000000 00000000 00000000 00000000 00000000
R7: 0xd0158640:
8640 00000001 00000001 00000002 00000000 00000000 00000000 00000000 00000000
8660 00000000 00000000 00000000 00000000 00000000 d407e140 00000000 00000000
8680 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
86a0 00000000 d01586a4 d01586a4 d01586ac d01586ac d22f34a4 00000000 00000000
86c0 d01586c0 d01586c0 d401d4e0 d22fa558 c065ca64 00000000 00000000 00000000
86e0 00000002 00000002 00000003 00000000 00000000 00000000 00000000 00000000
8700 00000000 00000000 00000000 00000000 00000000 d407f560 00000000 00000000
8720 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
Process SurfaceFlinger (pid: 2300, stack limit = 0xd024a2f0)
Stack: (0xd024bf30 to 0xd024c000)
bf20: 00000000 00000000 00000001 00000001
bf40: d41985a0 00000000 00004bc5 00000000 c08ee930 c08740c0 a8727958 04b91373
bf60: 00000000 00000010 40568d30 00000001 d41fe440 c007cc28 d4198588 d4198588
bf80: 00000008 41443548 ffffffff 00000000 000000fc c0048a84 d024a000 00000000
bfa0: 00000000 c0048900 41443548 ffffffff 0000000b 40568d30 00000010 ffffffff
bfc0: 41443548 ffffffff 00000000 000000fc 00000000 00000014 4144355c 00000000
bfe0: 401c5ff4 40568ce8 401c0b0d 40154f20 20000010 0000000b ffffffff ffffffff
Code: bad PC value
VPU blocking: timeout.
---[ end trace 1bd335430a63c09e ]---
Kernel panic - not syncing: Fatal exception
[<c004f9e4>] (unwind_backtrace+0x0/0x138) from [<c06454fc>] (panic+0x74/0x18c)
[<c06454fc>] (panic+0x74/0x18c) from [<c004c454>] (die+0x218/0x284)
[<c004c454>] (die+0x218/0x284) from [<c06452f0>] (__do_kernel_fault.part.3+0x54/0x74)
[<c06452f0>] (__do_kernel_fault.part.3+0x54/0x74) from [<c0053778>] (do_page_fault+0x2b4/0x31c)
[<c0053778>] (do_page_fault+0x2b4/0x31c) from [<c00424ac>] (do_PrefetchAbort+0x34/0x9c)
[<c00424ac>] (do_PrefetchAbort+0x34/0x9c) from [<c00484d4>] (__pabt_svc+0x74/0xc0)
Exception stack(0xd024bee8 to 0xd024bf30)
bee0: fffffffc d4202420 00000000 d41fe440 00000010 d024a000
bf00: 40568d30 d01586c0 00000010 00000001 ffffffff 00000001 d024bec8 d024bf30
bf20: c06499f0 00000000 60000013 ffffffff
[<c00484d4>] (__pabt_svc+0x74/0xc0) from [<c06499f0>] (__schedule+0x2ac/0x788)
CPU1: stopping
[<c004f9e4>] (unwind_backtrace+0x0/0x138) from [<c00423a8>] (do_IPI+0x1d4/0x208)
[<c00423a8>] (do_IPI+0x1d4/0x208) from [<c004834c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xc2b83de8 to 0xc2b83e30)
3de0: c08e8ccc 60000093 c089e148 c089e148 c08e8cd6 c08e8ced
3e00: c089e0e8 c08e8c18 0000001d c08e8cd6 00000001 60000013 00000000 c2b83e30
3e20: c008254c c0082660 60000013 ffffffff
[<c004834c>] (__irq_svc+0x4c/0xe8) from [<c0082660>] (vprintk+0x328/0x4a8)
[<c0082660>] (vprintk+0x328/0x4a8) from [<c0645630>] (printk+0x1c/0x2c)
[<c0645630>] (printk+0x1c/0x2c) from [<c0459290>] (vpu_ioctl+0x850/0x8f8)
[<c0459290>] (vpu_ioctl+0x850/0x8f8) from [<c0130a48>] (do_vfs_ioctl+0x80/0x54c)
[<c0130a48>] (do_vfs_ioctl+0x80/0x54c) from [<c0130f4c>] (sys_ioctl+0x38/0x5c)
[<c0130f4c>] (sys_ioctl+0x38/0x5c) from [<c0048900>] (ret_fast_syscall+0x0/0x30)
CPU: Freescale i.MX6 family TO1.5 at 792 MHz
Thermal sensor with ratio = 190
Temperature: 75 C, calibration data 0x5b14f57d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
Best regards
echo
 
					
				
		
 lily_zhang
		
			lily_zhang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello, Echo:
Because you are using one older release, recommend to consider to check whether the following patches are integrated:
- From log, it seems data corruption may happen in video playback case. So please consider to check whether all known ARM errata fixes are integrated.
- Please check whether DDR is stable enough.
- Please check whether ARM/SOC/PU voltage settings are aligned with latest datasheet.
- Please try to upgrade GPU version. GPU upgrade to latest p13 for JB4.2.2_1.1.0 release
You can also try the following tests to narrow down possible reasons:
- Disable all power saving technology. Disable CPU Frequency etc.
- Disable system to enter WAIT mode.
- Try to disable VPU clock off operation.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi echo
please follow recommendations provided for similar issue on
https://community.freescale.com/thread/323018
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
I do get unuserful information from similar issue your provided.
Running OS is android, so I can not change the kernel version.
I just want you provide us a fixed this issue way base on android 4.2.2.
Have any patch or fix method base on android 4.2.2(kernel 3.0.35)?
I saw many questions about similar vpu issues asked on nxp community, but look like has no satisfied answer.
Thanks.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi echo
as stated on suggested link this issue is well known in
kernel 3.0.35 and there are no workarounds or solutions for it.
Experts suggest to move on latest kernels where it is fixed.
Hope you will find this info as userful.
Best regards
igor
Hi igorpadykov,
According to your suggestion, can we only replace 3.0.35 kernel to latest kernel base on Android 4.2.2?
Or must we update newer Android OS(such as 5.0....) including latest kernel? How about your opinion?
Thanks.