vAnalyzer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vAnalyzer

2,481 Views
manoje_s_
Contributor III

I am developing an OpenGL ES 2.0 application in QNX 6.0 OS running on IMX6 Quad+

I wanted to analyze the performance using the vAnalyzer and therefore can someone share the details about how this can be done in the QNX environment?

Labels (2)
0 Kudos
Reply
1 Reply

2,229 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Manoj,

vAnalyzer is, like all other tools in the VTK, a Windows application, which is a bit unfortunate since most i.MX boards probably run Linux, and hence the developers probably run Linux on their desktop machine as well. Fortunately, it runs fine under Wine, simply running wine setup.exe will install vAnalyzer.

You can see the steps to use vAnalyzer in Linux, which I think you can apply in QNX, which NXP does not support. 

How to Profile QtQuick applications on Freescale i.MX 6 with vAnalyzer - KDAB 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply