MCIMX6UL-EVK main (CPU) board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6UL-EVK main (CPU) board

541 Views
seuruguillaume
Contributor I

I would like to use the MCIMX6UL-EVK main board (CPU+memories) with a custom base board.

Is it something possible?

Is the main board available without buying the whole EVKB (main board + base board)?

Or do I need to use another IMX6 SOM?

Thanks

Labels (2)
0 Kudos
1 Reply

447 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Seuru,

I don't think it is available without the baseboard but you may contact your distributor.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos