use udhcpc will close other interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use udhcpc will close other interface

1,181 Views
HenryHsu
Contributor I

My BSP version is 5.10.72 and use IMX6DL.

When i use udhcpc to get IP address, it will close down other internet at first time.

same problem as below link:

https://community.nxp.com/t5/i-MX-Processors/yocto-udhcpc-problem/m-p/1759415

For example:

I use udhcpc -i wwan0 command and my eth0, eth1 will be down.

Is this problem same as the known issue in release note? but my image is in emmc not sd card.

螢幕擷取畫面 2024-04-15 144210.png

Is there any solution and why dose this problem happen?

 

Labels (1)
0 Kudos
Reply
2 Replies

1,157 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @HenryHsu 

Is this problem same as the known issue in release note?

-->It's not different.

When i use udhcpc to get IP address, it will close down other internet at first time.

-->For this issue, it may caused by udhcpc scripts and there is no solution. The previous link has already escalated for SE team and no solution.

0 Kudos
Reply

1,154 Views
HenryHsu
Contributor I

Hi,Zhiming_Liu

Thank you for the reply.

 

0 Kudos
Reply