use udhcpc will close other interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use udhcpc will close other interface

1,789件の閲覧回数
HenryHsu
Contributor I

My BSP version is 5.10.72 and use IMX6DL.

When i use udhcpc to get IP address, it will close down other internet at first time.

same problem as below link:

https://community.nxp.com/t5/i-MX-Processors/yocto-udhcpc-problem/m-p/1759415

For example:

I use udhcpc -i wwan0 command and my eth0, eth1 will be down.

Is this problem same as the known issue in release note? but my image is in emmc not sd card.

螢幕擷取畫面 2024-04-15 144210.png

Is there any solution and why dose this problem happen?

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,765件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @HenryHsu 

Is this problem same as the known issue in release note?

-->It's not different.

When i use udhcpc to get IP address, it will close down other internet at first time.

-->For this issue, it may caused by udhcpc scripts and there is no solution. The previous link has already escalated for SE team and no solution.

0 件の賞賛
返信

1,762件の閲覧回数
HenryHsu
Contributor I

Hi,Zhiming_Liu

Thank you for the reply.

 

0 件の賞賛
返信