use of aes, sha algorithms api

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use of aes, sha algorithms api

1,549 Views
manivannanm
Contributor I

hi all,

           i am having free scale sabre auto board with i.mx6 arm v9 processor. i found that this boad has cryptographic accelerators which contains AES-128/256 ,Hash & HMAC: MD5, SHA-1, SHA-224, SHA-256 algorithms. i need to use those algorithms. so i need libraries and APIs of those algorithms. can anyone help me by where those libraries are found and how to use those. Thanks in advance.

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,402 Views
Yuri
NXP Employee
NXP Employee

  The i.MX6  cryptographic accelerator CAAM is supported in Linux, and  the CAAM driver
is integrated with the Linux Crypto API.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,402 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). Be aware that to give you remote support through a SR, we will still need the confirmation of a Freescale employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SR and name us a Freescale person that can confirm this. If you have not signed an agreement, please contact your local Freescale Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS

Hope this will be useful for you
Best regards!
/Carlos

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply