use mfgtool to upgrade rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use mfgtool to upgrade rootfs

1,238件の閲覧回数
yufe
Contributor II

my custom board have mfg tool  to download firmware(have no ethernet port).I must use mfgtool to download whole rootfs even just modified only one file, it's a waste of time. Is there a convenient way to upgrade rootfs with mfgtool?

タグ(1)
0 件の賞賛
返信
1 返信

1,028件の閲覧回数
art
NXP Employee
NXP Employee

Only the whole rootfs image can be reloaded with the MFGtool. If you only need to add a couple of files to your board's rootfs, better seems to use some external mass storage device, e.g. an USB Flash drive.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------