use mfgtool to upgrade rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

use mfgtool to upgrade rootfs

1,230 次查看
yufe
Contributor II

my custom board have mfg tool  to download firmware(have no ethernet port).I must use mfgtool to download whole rootfs even just modified only one file, it's a waste of time. Is there a convenient way to upgrade rootfs with mfgtool?

标记 (1)
0 项奖励
回复
1 回复

1,020 次查看
art
NXP Employee
NXP Employee

Only the whole rootfs image can be reloaded with the MFGtool. If you only need to add a couple of files to your board's rootfs, better seems to use some external mass storage device, e.g. an USB Flash drive.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------