usb host stack support for 4G modem device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb host stack support for 4G modem device

ソリューションへジャンプ
2,808件の閲覧回数
sbabu
Contributor III

Dear All,

Just wanted to check if the USB host stack available in MCUXpresso SDK supports 4G modem type devices. Also SFTP protocol as i don't see any SFTP protocol in lwip stack in the SDK.

Thanks

Babu

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,775件の閲覧回数
sbabu
Contributor III

Hi Chavira,

We are using MX RT1024.

Thanks,

Subash

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,700件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi again @sbabu,

I believe this Application Note will be useful for your inquiry: https://www.nxp.com/docs/en/application-note/AN13940.pdf

 

0 件の賞賛
返信
2,725件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @sbabu,

The SFTP protocol is not supported. As for the 4G modem type devices, I believe it depend on the USB class type required for your modem. As long as it is a supported class, it should be OK.

BR,
Edwin.

0 件の賞賛
返信
2,784件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

Are you using iMX8 or iMXRT?

0 件の賞賛
返信
2,776件の閲覧回数
sbabu
Contributor III

Hi Chavira,

We are using MX RT1024.

Thanks,

Subash

0 件の賞賛
返信