usb host stack support for 4G modem device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb host stack support for 4G modem device

Jump to solution
2,774 Views
sbabu
Contributor III

Dear All,

Just wanted to check if the USB host stack available in MCUXpresso SDK supports 4G modem type devices. Also SFTP protocol as i don't see any SFTP protocol in lwip stack in the SDK.

Thanks

Babu

 

 

Labels (1)
0 Kudos
Reply
1 Solution
2,741 Views
sbabu
Contributor III

Hi Chavira,

We are using MX RT1024.

Thanks,

Subash

View solution in original post

0 Kudos
Reply
4 Replies
2,666 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi again @sbabu,

I believe this Application Note will be useful for your inquiry: https://www.nxp.com/docs/en/application-note/AN13940.pdf

 

0 Kudos
Reply
2,691 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @sbabu,

The SFTP protocol is not supported. As for the 4G modem type devices, I believe it depend on the USB class type required for your modem. As long as it is a supported class, it should be OK.

BR,
Edwin.

0 Kudos
Reply
2,750 Views
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

Are you using iMX8 or iMXRT?

0 Kudos
Reply
2,742 Views
sbabu
Contributor III

Hi Chavira,

We are using MX RT1024.

Thanks,

Subash

0 Kudos
Reply