undefined reference to `imx_add_mipi_dsi' `imx6q_mipi_dsi_data'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

undefined reference to `imx_add_mipi_dsi' `imx6q_mipi_dsi_data'

跳至解决方案
2,168 次查看
jiangshao
Contributor V

最近因为对应mipi接口的lcd,在/kernel_imx/arch/arm/mach-mx6/board-mx6q_sabresd.c中打开
imx6q_add_mipi_dsi(&mipi_dsi_pdata);的注释

// change by shao, 2016-11-16
// imx6q_add_mipi_dsi(&mipi_dsi_pdata);
imx6q_add_mipi_dsi(&mipi_dsi_pdata);

内核配置中,CONFIG_FB_MXC_MIPI_DSI=y

编译出现了错误:
arch/arm/mach-mx6/built-in.o: In function `mx6_sabresd_board_init':
/media/myandroid/work/20161018newB/kernel_imx/arch/arm/mach-mx6/board-mx6q_sabresd.c:2272: undefined reference to `imx_add_mipi_dsi'
/media/myandroid/work/20161018newB/kernel_imx/arch/arm/mach-mx6/board-mx6q_sabresd.c:2474: undefined reference to `imx6q_mipi_dsi_data'
make: *** [.tmp_vmlinux1] 错误 1

而确认board-mx6q_sabresd.c包含的头文件devices-imx6q.h中,明明有如下定义:
extern const struct imx_mipi_dsi_data imx6q_mipi_dsi_data __initconst;
#define imx6q_add_mipi_dsi(pdata) \
imx_add_mipi_dsi(&imx6q_mipi_dsi_data, pdata)

且devices-imx6q.h包含的头文件/kernel_imx/arch/arm/plat-mxc/include/mach/devices-common.h
中,也有如下定义:
#include <mach/mipi_dsi.h>
struct imx_mipi_dsi_data {
int id;
resource_size_t iobase;
resource_size_t iosize;
resource_size_t irq;
};
struct platform_device *__init imx_add_mipi_dsi(
const struct imx_mipi_dsi_data *data,
const struct mipi_dsi_platform_data *pdata);

make distclean也都试过了,错误依旧,

有哪位知道为什么吗?

标签 (4)
0 项奖励
回复
1 解答
1,752 次查看
jiangshao
Contributor V

终于找到问题所在了!

从/kernel_imx/arch/arm/mach-mx6/Kconfig可以看出,MACH_MX6Q_SABRESD下没有

select IMX_HAVE_PLATFORM_IMX_MIPI_DSI

加上或者在内核中选中那个i.MX6Quad Armadillo2 platform亦可

仅供参考

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,753 次查看
jiangshao
Contributor V

终于找到问题所在了!

从/kernel_imx/arch/arm/mach-mx6/Kconfig可以看出,MACH_MX6Q_SABRESD下没有

select IMX_HAVE_PLATFORM_IMX_MIPI_DSI

加上或者在内核中选中那个i.MX6Quad Armadillo2 platform亦可

仅供参考

0 项奖励
回复
1,752 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  jiang

please try to make build from scratch on new VM,

also recommended to start with minimal configuration.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复