uboot porting to LPDDR2 on imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot porting to LPDDR2 on imx6ull

1,456 Views
vladimirchernin
Contributor III

Hi!

Our board custom design based on mx6ullevk ref board working with DDR3 500mb 

we must use with LPDDR2 Alliance AS4C128M16MD2-25BCN  256mb 

in uboot source under /board/freescale/mx6ullevk i see imximage_lpddr2.cfg

seems to be lpddr2 DCD config

Can i use  imximage_lpddr2.cfg with my LPDDR2?

Thanks

Vladimir

Labels (3)
0 Kudos
Reply
3 Replies

1,248 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vladimir

for new board recommended to run ddr tester

i.MX6/7 DDR Stress Test Tool V2.80 

and populate imximage_lpddr2.cfg with new calibration coefficients

found from tester. Use

https://community.nxp.com/docs/DOC-333933 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,248 Views
vladimirchernin
Contributor III

Hi Igor!

Please explain if i can use it for any of LPDDR2 from any manufacturer?

is it size dependent? 

my DDR is 256MB

Thanks

Vladimir

 

0 Kudos
Reply

1,248 Views
igorpadykov
NXP Employee
NXP Employee

no, for every new memory new calibartion coefficients should be found using ddr tester.

Best regards
igor

0 Kudos
Reply