uboot plugin mode used in HAB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uboot plugin mode used in HAB

1,014 次查看
liuhao1
Contributor II

My project want to use seucre boot at imx6d

Current project use mx6q_4x_mt41j128.cfg with CONFIG_USE_PLUGIN

But It seem if I want to use thesecureboot  fuction.I need undef CONFIG_USE_PLUGIN

1.Could it have some introduce about the uboot plugin mode ?

2.If I want to add the secure boot fuse with uboot plugin mode.what could I do ?
3.if I use the DCDmode.How can I trans the plugin config to cfg file

0 项奖励
回复
1 回复

946 次查看
igorpadykov
NXP Employee
NXP Employee

Hi liuhao

please create service request for obtaining additional information

https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复