uboot mfgtool failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uboot mfgtool failed

2,123 次查看
likangmao
Contributor I

Hi, Community:

I will to burn uboot into the board for i.MX6Solo/DualLite by MFGTools(Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER), errors :

ModuleID[2] LevelID[1]: CmdOpreation[0]--set m_hDeviceArriveEvent.
ModuleID[2] LevelID[10]: CmdOpreation[0]--WaitforEvents device arrive1
ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\likangmao\imx6\L3.14.52_1.1.0_ga-mfg-tools\mfgtools\Profiles\Linux\OS Firmware\firmware\u-boot-imx6dlsabreauto_nand.imx

stop here,

There are no outputs in serial port

标记 (1)
0 项奖励
回复
1 回复

1,986 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 康茂 李

for new board mfg tools firmware (files in /firmware folder) should be
updated with new ddr calibration coefficients found from ddr test:
i.MX6/7 DDR Stress Test Tool V2.90 
put them to uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg and
rebuild firmware using procedure described in sect.6.2 Manufacturing Tool, MFGTool
attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复