uboot logo color is not normal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot logo color is not normal

Jump to solution
91,512 Views
fulinux
Contributor IV

Dear Community,

board: imx6q;

version: u-boot-2009.08;

i did what this doc said: https://community.nxp.com/docs/DOC-98109

but the logo color is not normal, it si green like this:

P60512-190156.jpg

what is wrong? and this is my head file:

    //#define IPU_OUTPUT_MODE_HDMI

    #define IPU_OUTPUT_MODE_LVDS

//  #define IPU_OUTPUT_MODE_LCD

#ifdef IPU_OUTPUT_MODE_LVDS

    // For LVDS, 1920*1080 resolution, dual channel

    #define DISPLAY_WIDTH   1920

    #define DISPLAY_HEIGHT  1080

    #define DISPLAY_BPP     32

    #define DISPLAY_IF_BPP  24  // RGB24 interface

    #define DISPLAY_HSYNC_START 80

    #define DISPLAY_HSYNC_END       68

    #define DISPLAY_HSYNC_WIDTH 12

    #define DISPLAY_VSYNC_START 15

    #define DISPLAY_VSYNC_END   15

    #define DISPLAY_VSYNC_WIDTH 8

#define DISPLAY_PIX_CLOCK   139526400  //(DISPLAY_HSYNC_START + DISPLAY_HSYNC_END + DISPLAY_HSYNC_WIDTH + DISPLAY_WIDTH) *   

(DISPLAY_VSYNC_START + DISPLAY_VSYNC_END + DISPLAY_VSYNC_WIDTH + DISPLAY_HEIGHT) * refresh rate (60Hz)

    #define LVDS_SPLIT_MODE  // For dual channel split mode.

    #define DISPLAY_VSYNC_POLARITY          1

    #define DISPLAY_HSYNC_POLARITY          1

    #define DISPLAY_CLOCK_POLARITY          1

    #define DISPLAY_DATA_POLARITY               0

    #define DISPLAY_DATA_ENABLE_POLARITY        1

    #define IPU_NUM         1  // 1 for IPU1, 2 for IPU2.

    #define DI_NUM          0  // 0 for DI0, 1 for DI1.

    #define LVDS_PORT       0  // 0 for LVDS0, 1 for LVDS1.

    #define DI_CLOCK_EXTERNAL_MODE  //When clock external mode was defined, the DI clock root will be PLL3 PFD1,

                                //without this macro, the DI root clock is IPU internal clock.

nothing changed, just above, can you help me? what should i do? what is info do you need? tell me.

wating for your reply?

thank you.

fulinux.

Labels (1)
Tags (2)
1 Solution
87,219 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

I had identified the issue, please apply the attached uboot patch to fix it.

it is based on JB4.3_1.1.1_uboot_logo_keep_patch_2015-09-18.zip

View solution in original post

0 Kudos
Reply
46 Replies
73,522 Views
fulinux
Contributor IV

kernel logo can show ppm file not bmp file, it is not logo file's problem, when i write 0x00 to fb memory is also little white. i have told you above. it is very strange.

0 Kudos
Reply
73,522 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

In linux, you can use dd command to show the bmp file to frame buffer:

dd if=logo.bmp of=/dev/fb0 bs=1 skip=54

You'd better find out the different display setting in your kernel and uboot.

0 Kudos
Reply
73,522 Views
jiejia
Contributor III

Dear Qiang,

I have the same problem. It may have some problem with the 0001-Enable-uboot-logo-for-HDMI-LCD-and-LVDS.patch.  The LVDS CLK  is about 75M no matter what the DISPLAY_PIX_CLOCK is. Woud you mind testing for what I said?

0 Kudos
Reply
73,522 Views
fulinux
Contributor IV

Dear Qiang,

i did as you said, i shows well:

P60516-154851.jpg

do you need any information? pls tell me.

thank you,

fulinux.

0 Kudos
Reply
73,522 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Maybe there is some wrong porting code in your uboot.

0 Kudos
Reply
73,522 Views
fulinux
Contributor IV

Hi, do you need my uboot code?

0 Kudos
Reply
73,522 Views
fulinux
Contributor IV

OK, i will test as you said;

and look at this:

pData = (unsigned char *)CONFIG_FB_BASE; CONFIG_FB_BASE = 0x27B00000

and i have write 0x00000 from 0x27B00000 to 0x27B00000 + bmp file size. and read memory by "md" command it shows right:

MX6Q SABRESD U-Boot > md 0x27B00000

27b00000: 00000000 00000000 00000000 00000000    ................

27b00010: 00000000 00000000 00000000 00000000    ................

27b00020: 00000000 00000000 00000000 00000000    ................

27b00030: 00000000 00000000 00000000 00000000    ................

....

but now, the lcd panel is still litte white:

P60513-154733.jpg

but it is not more white than when i write 0xfffffff to fb memory. i don't know if you know what i mean.

thank you,

fulinux.

0 Kudos
Reply
73,521 Views
fulinux
Contributor IV

Hi Qiang,

with my kernel attach file

0 Kudos
Reply
73,524 Views
fulinux
Contributor IV

hi Qiang,

is it wrong with my backlight and lcd power settings of gpios, this is my settings:

at setup_lvds_iomux() function in board/freescale/mx6q_sabresd/mx6q_sabresd.c:

#if defined CONFIG_MX6Q

    /* GPIO backlight */

    //mxc_iomux_v3_setup_pad(MX6Q_PAD_SD1_DAT3__PWM1_PWMO);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_9__PWM1_PWMO);

    /* LVDS panel CABC_EN */

    mxc_iomux_v3_setup_pad(MX6Q_PAD_NANDF_CS2__GPIO_6_15);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_NANDF_CS3__GPIO_6_16);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_2__GPIO_1_2);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_7__GPIO_1_7);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_19__GPIO_4_5);

    reg = readl(GPIO6_BASE_ADDR + GPIO_DR);

    reg &= ~(1 << 16);

    writel(reg, GPIO6_BASE_ADDR + GPIO_DR);

#if 1

    gpio_direction_output(IMX_GPIO_NR(1, 2), 1);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(1, 2), 0);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(1, 2), 1);

    gpio_direction_output(IMX_GPIO_NR(4, 5), 1);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(4, 5), 1);

    gpio_direction_output(IMX_GPIO_NR(1, 7), 0);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(1, 7), 0);

#endif

at board_late_init() function:

    ipu_display_setup();

    gpio_set_value(IMX_GPIO_NR(1, 7), 1);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(4, 5), 0);

Do you think that was right?

with my attach file.

0 Kudos
Reply
73,532 Views
fulinux
Contributor IV

Hi,

when i modified this:

    #define DISPLAY_WIDTH  1920

    #define DISPLAY_HEIGHT  1080

    #define DISPLAY_BPP    32

    #define DISPLAY_IF_BPP  24  // RGB24 interface

    #define DISPLAY_HSYNC_START 80

    #define DISPLAY_HSYNC_END  68

    #define DISPLAY_HSYNC_WIDTH 12

    #define DISPLAY_VSYNC_START 15

    #define DISPLAY_VSYNC_END  15

    #define DISPLAY_VSYNC_WIDTH 8

    #define DISPLAY_PIX_CLOCK  139526400  //(DISPLAY_HSYNC_START + DISPLAY_HSYNC_END + DISPLAY_HSYNC_WIDTH + DISPLAY_WIDTH) *    

(DISPLAY_VSYNC_START + DISPLAY_VSYNC_END + DISPLAY_VSYNC_WIDTH + DISPLAY_HEIGHT) * refresh rate (60Hz)

    #define LVDS_SPLIT_MODE  1  // For dual channel split mode.

#endif

    #define DISPLAY_VSYNC_POLARITY          0

    #define DISPLAY_HSYNC_POLARITY          0

    #define DISPLAY_CLOCK_POLARITY          1

    #define DISPLAY_DATA_POLARITY              0

    #define DISPLAY_DATA_ENABLE_POLARITY        1

    #define IPU_NUM        1  // 1 for IPU1, 2 for IPU2.

    #define DI_NUM          0  // 0 for DI0, 1 for DI1.

    #define LVDS_PORT      1  // 0 for LVDS0, 1 for LVDS1.

    #define DI_CLOCK_EXTERNAL_MODE  //When clock external mode was defined, the DI clock root will be PLL3 PFD1,

                                //without this macro, the DI root clock is IPU internal clock.

and

    bmpReady = 0;

    if (bmpReady == 0) {

        // Fill RGB frame buffer

        // Red

        for (i = 0; i < (DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8) / 3); i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0x00;

            pData[i + 1] = 0xF8;

#else

and the lcd panel screen display like this:

P60513-152541.jpg

you can look at this, the color is lighter;

when i change code like this, change "pData[] = 0x FF" to 0x00:

        // Red

        for (i = 0; i < (DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8) / 3); i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0x00;

            pData[i + 1] = 0xF8;

#else

            pData[i + 0] = 0x00;

            pData[i + 1] = 0x00;

            pData[i + 2] = 0x00;

            pData[i + 3] = 0x00;

#endif

        }

        // Green

        for (; i < (DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8) / 3) * 2; i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0xE0;

            pData[i + 1] = 0x07;

#else

            pData[i + 0] = 0x00;

            pData[i + 1] = 0x00;

            pData[i + 2] = 0x00;

            pData[i + 3] = 0x00;

#endif

        }

        // Blue

        for (; i < DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8); i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0x1F;

            pData[i + 1] = 0x00;

#else

            pData[i + 0] = 0x00;

            pData[i + 1] = 0x00;

            pData[i + 2] = 0x00;

            pData[i + 3] = 0x00;

then like this:

P60513-154733.jpg

it should be black,but it is whilt!

0 Kudos
Reply
73,532 Views
huaweiyu
Contributor I

hi,

could you tell me the path of file where you insert  bmpReady = 0;

thank you

0 Kudos
Reply
73,532 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, from your kernel setting, the DE is high active, so it should be "#define DISPLAY_DATA_ENABLE_POLARITY  1"

For black to white issue, you can change DISPLAY_DATA_POLARITY from 0 to 1 to invert the data line.

I think all these informations should be found from your panel's datasheet.

0 Kudos
Reply
73,532 Views
fulinux
Contributor IV

when it should be black it shows white, but when it should be whilt it shows more white, so it can't shows black.

when i change "#define IPU_NUM 1" to 2,it shows white, red and blue looply, why

0 Kudos
Reply
73,532 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Another thing can be tried: invert the clock polarity, change DISPLAY_CLOCK_POLARITY from 1 to 0.

The display shows white, red and blue looply, that means the panel hasn't found valid input signal and show its test pattern.

0 Kudos
Reply
73,532 Views
fulinux
Contributor IV

it dosen't change anything when i change DISPLAY_CLOCK_POLARITY from 1 to 0. this is logo picture(original picture):

254-1401010Z511.jpg

this is the screen shows:

P60513-163732.jpg

0 Kudos
Reply
73,532 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Can you attach your bmp file and panel datasheet here?

0 Kudos
Reply
73,506 Views
fulinux
Contributor IV

Yes ^_^ !

ps.

logo.bmp-bak file: this file i have skiped 54bytes from logo.bmp;

0 Kudos
Reply
73,506 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

From the datasheet, the setting should be followed, no other issues found.

#define DISPLAY_VSYNC_POLARITY   0

#define DISPLAY_HSYNC_POLARITY   0

#define DISPLAY_CLOCK_POLARITY   0

#define DISPLAY_DATA_POLARITY    0

#define DISPLAY_DATA_ENABLE_POLARITY  1

0 Kudos
Reply
73,506 Views
fulinux
Contributor IV

Hi,

it doesn't change anything when i did as what you said. it still like this:

P60513-163732.jpg

i am trying uboot-2015.04(on branch imx_v2015.04_4.1.15_1.0.0_ga), how can i enable split mode in uboot-2015.04?

0 Kudos
Reply
73,506 Views
fulinux
Contributor IV

Dear all,

can anybody help me? how can i solve this problem?

fulinux.

0 Kudos
Reply
73,506 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

How about your hardware connection?

Do you just used three pair of LVDS data lane? If so, you should set "#define DISPLAY_IF_BPP  24 " to 18.

0 Kudos
Reply