uboot lcd RGB888

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot lcd RGB888

2,385件の閲覧回数
强王
Contributor IV

目前使用hsd070IDW1-E13 LCD RGB888的显示屏,目前UBOOT不显示LOGO,

我把LCD的配置打开,还是不显示LOGO,内核显示一切正常

需要怎么配置

UBOOT:2014.04

ラベル(3)
0 件の賞賛
返信
1 返信

2,131件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you share your setting code? or you can refer to the code as below, this setting is for mx53, you can refer to it.

According to the datasheet of HSD070IDW1-A20 , video mode should be :

struct fb_videomode {

name = “HSD-WVGA”;

refresh = 30000000/(928*525)=62 ;

xres = 800;

yres = 480;

pixclock = 1/30000000 * 10e12 =33333 ;

left_margin = 40;

right_margin = 40;

upper_margin = 29;

lower_margin; = 13

hsync_len = 48 ;

vsync_len = 3;

sync = FB_SYNC_CLK_LAT_FALL ;

vmode = FB_VMODE_NONINTERLACED ;

flag = 0;

};

      So the video mode for new LCD is :

struct fb_videomode video_modes {

            /* 800x480 @ 62 Hz , pixel clk @ 30MHz */

“HSD-WVGA”, 62, 800, 480, 33333, 40,40,29,13,48,3,

FB_SYNC_CLK_LAT_FALL,

FB_VMODE_NONINTERLACED,

0,

};

static struct mxc_fb_platform_data fb_data[] = {

      {

      .interface_pix_fmt = IPU_PIX_FMT_RGB24,

      .mode_str = "HSD-WVGA",

      .mode = video_modes,

      .num_modes = ARRAY_SIZE(video_modes),

      },

};

0 件の賞賛
返信