uboot i2c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot i2c

1,631 Views
yuhundehao
Contributor III

platform :imx6q

uboot:2009

kernel:3.0.0.5

The same chip needs 6S to initialize I2C in uboot and 1s to initialize this chip in kernel driver. Why?

0 Kudos
Reply
2 Replies

1,610 Views
art
NXP Employee
NXP Employee

Most likely, this is the issue in the Uboot code. Try to migrate to the later version of Uboot.

Best Regards,
Artur

0 Kudos
Reply

1,607 Views
yuhundehao
Contributor III
Thanks ! The uboot migrate is later version that solve this problem。 I kept the status quo and didn't solve it。
0 Kudos
Reply