uboot i2c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot i2c

2,273件の閲覧回数
yuhundehao
Contributor III

platform :imx6q

uboot:2009

kernel:3.0.0.5

The same chip needs 6S to initialize I2C in uboot and 1s to initialize this chip in kernel driver. Why?

0 件の賞賛
返信
2 返答(返信)

2,252件の閲覧回数
art
NXP Employee
NXP Employee

Most likely, this is the issue in the Uboot code. Try to migrate to the later version of Uboot.

Best Regards,
Artur

0 件の賞賛
返信

2,249件の閲覧回数
yuhundehao
Contributor III
Thanks ! The uboot migrate is later version that solve this problem。 I kept the status quo and didn't solve it。
0 件の賞賛
返信