ubifs_scan: corrupt empty space at LEB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ubifs_scan: corrupt empty space at LEB

2,307 Views
xavierdouville
Contributor II

Hi

Using NXP i.MX 6ULL (Digi ccimx6ul) and kernel 5.4.84, I get the following error when trying to mount a ubifs:

UBIFS error (ubi1:0 pid 910): ubifs_scan: corrupt empty space at LEB 104:118784
UBIFS error (ubi1:0 pid 910): ubifs_scanned_corruption: corruption at LEB 104:118784
UBIFS error (ubi1:0 pid 910): ubifs_scanned_corruption: first 8192 bytes from LEB 104:118784
UBIFS error (ubi1:0 pid 910): ubifs_scan: LEB 104 scanning failed
mount: mounting ubi1:update on /mnt/update/ failed: Structure needs cleaning

 

I've seen a couple reports of similar problems and some old patches, but they do not apply to recent kernel versions.

Is there something I can do to allow this filesystem to mount and recover at least some of the data?

Is there anything to do to prevent this problem from happening again in the future?

 

thanks

 

Xavier Douville

 

Tags (3)
0 Kudos
Reply
1 Reply

1,728 Views
xavierdouville
Contributor II

nobody? Has this been fixed in recent kernels?

0 Kudos
Reply