ubifs_scan: corrupt empty space at LEB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ubifs_scan: corrupt empty space at LEB

2,369件の閲覧回数
xavierdouville
Contributor II

Hi

Using NXP i.MX 6ULL (Digi ccimx6ul) and kernel 5.4.84, I get the following error when trying to mount a ubifs:

UBIFS error (ubi1:0 pid 910): ubifs_scan: corrupt empty space at LEB 104:118784
UBIFS error (ubi1:0 pid 910): ubifs_scanned_corruption: corruption at LEB 104:118784
UBIFS error (ubi1:0 pid 910): ubifs_scanned_corruption: first 8192 bytes from LEB 104:118784
UBIFS error (ubi1:0 pid 910): ubifs_scan: LEB 104 scanning failed
mount: mounting ubi1:update on /mnt/update/ failed: Structure needs cleaning

 

I've seen a couple reports of similar problems and some old patches, but they do not apply to recent kernel versions.

Is there something I can do to allow this filesystem to mount and recover at least some of the data?

Is there anything to do to prevent this problem from happening again in the future?

 

thanks

 

Xavier Douville

 

タグ(3)
0 件の賞賛
返信
1 返信

1,790件の閲覧回数
xavierdouville
Contributor II

nobody? Has this been fixed in recent kernels?

0 件の賞賛
返信