uImage for mfgtool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,084件の閲覧回数
kylekenj
Contributor III

Does anyone know where I could find the source for the uImage use in the mfgtool. It is found in Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware. Thanks.

Kyle

ラベル(3)
0 件の賞賛
返信
1 解決策
1,750件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kyle,

The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~

Best Regards

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,751件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kyle,

The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~

Best Regards

Dan

0 件の賞賛
返信