uImage for mfgtool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

uImage for mfgtool

跳至解决方案
2,088 次查看
kylekenj
Contributor III

Does anyone know where I could find the source for the uImage use in the mfgtool. It is found in Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware. Thanks.

Kyle

标签 (3)
0 项奖励
回复
1 解答
1,754 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kyle,

The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~

Best Regards

Dan

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,755 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kyle,

The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~

Best Regards

Dan

0 项奖励
回复