uImage for mfgtool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uImage for mfgtool

Jump to solution
2,087 Views
kylekenj
Contributor III

Does anyone know where I could find the source for the uImage use in the mfgtool. It is found in Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware. Thanks.

Kyle

Labels (3)
0 Kudos
Reply
1 Solution
1,753 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kyle,

The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~

Best Regards

Dan

View solution in original post

0 Kudos
Reply
1 Reply
1,754 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kyle,

The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~

Best Regards

Dan

0 Kudos
Reply