uBoot file structure?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uBoot file structure?

1,987件の閲覧回数
mikemandeville
Contributor II

what file within uBoot contains the non-default alt modes settings (ie iomux type settings) and where in the file structure It is located?

ラベル(4)
タグ(5)
0 件の賞賛
返信
1 返信

1,779件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mike

I think this is iomux.c, please check

Table 3   Related Source Files

AN4172 "U-Boot for i.MX35 based Designs"

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信