uBoot file structure?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uBoot file structure?

1,985 Views
mikemandeville
Contributor II

what file within uBoot contains the non-default alt modes settings (ie iomux type settings) and where in the file structure It is located?

Labels (4)
0 Kudos
Reply
1 Reply

1,777 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mike

I think this is iomux.c, please check

Table 3   Related Source Files

AN4172 "U-Boot for i.MX35 based Designs"

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply