u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot

1,807件の閲覧回数
saida
Contributor II

hi i.mx community

1. where i can see puts(),debug(),printf() defined source code and how it is working after seril_init() function ?

2. is there any hidden libraries in u-boot ?

3. where is dts file for sabresd dl board in u-boot ?

help in this regard

thank you

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,723件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi saida

for 1.2. one can post on uboot mail list:

U-Boot Info Page

regarding dts files, they are located in

linux_xxx/arch/arm/boot/dts/  folder

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,723件の閲覧回数
saida
Contributor II

thank you igorpadykov

you are always helpful to me

i am happy with you reply

0 件の賞賛
返信