u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

u-boot

1,802 次查看
saida
Contributor II

hi i.mx community

1. where i can see puts(),debug(),printf() defined source code and how it is working after seril_init() function ?

2. is there any hidden libraries in u-boot ?

3. where is dts file for sabresd dl board in u-boot ?

help in this regard

thank you

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,718 次查看
igorpadykov
NXP Employee
NXP Employee

Hi saida

for 1.2. one can post on uboot mail list:

U-Boot Info Page

regarding dts files, they are located in

linux_xxx/arch/arm/boot/dts/  folder

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,718 次查看
saida
Contributor II

thank you igorpadykov

you are always helpful to me

i am happy with you reply

0 项奖励
回复