u-boot in i.MX93 EVK and changing device tree blob (dtb)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot in i.MX93 EVK and changing device tree blob (dtb)

3,174 Views
bitspirate
Contributor III

Hi NXP Staff,

My goal was to modify the device tree that the kernel starts to activate the LVDS panel.

Now, I tried several ways and I fail to understand what is going on in u-boot-imx. Using devtool shows that only imx93-11x11-evk.dts is available, however I cannot find where the other dtbs are built.

Trying to set a different dts will obviously fail, since u-boot cannot find it. Unfortunately I am failing at figuring out where the other dtbs are built (in my deploy dir there are plenty of other dtbs).

Initially, I thought it would just require to modify any of the following variables:

UBOOT_DTB_NAME = "imx93-11x11-evk-boe-wxga-lvds-panel.dtb"
KERNEL_DEVICETREE_BASENAME = "imx93-11x11-evk-boe-wxga-lvds-panel"
 
This does not work, either by bbappend or local.conf. The result is always imx93-11x11-evk. Where or how is the right way/place to modify the device tree that is passed to the kernel?
 
Thanks
Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

3,146 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @bitspirate

Thank you for contacting NXP Support. 

Here is a link to an article that you could find especially useful to properly compile your device tree:
How to use Devshell to compile device tree files. - NXP Community

To set the device tree on your board you will need to edit the variable environment for device tree on U-Boot using the following commands:

1. Use fatls <interface> <device[:partition]> [<directory>]

fatls mmc 1:1
(Device 1 : Partition 1)

With this command, we will be able to list device tree files.

=> fatls mmc 1:1

2. Select your device tree "imx93-lvds.dtb" and use the command editenv fdtfile

=> editenv fdtfile
Output example
edit: imx93-lvds.dtb

3. In edit command line put the selected device tree .dtb
4. Use saveenv command to save environment and continue with the boot process.

I hope this information will be helpful. 

Have a great day!

0 Kudos
Reply